Feedback_Source_PPR
Feedback_Source_PPR
| Address: | 10250 (280AH) |
| Type: | Unsigned32 |
| Access: | Read/Write |
| Unit: | Inc |
| Range: | Unsigned32 |
| Default Value: | 1600 |
| Store Supported: | Yes |
| Description: | This value is used for Feedback feature and define the quadrature pulses per revolution of incremental encoder installed on motor rear shaft. |
| Notes: | See Closed Loop Modality for details. |